AXIS#.LOAD.INERTIA

Description

AXIS#.LOAD.INERTIA sets the load inertia.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

kgcm² for rotary motors

Range

1 to 1,000,000 kgcm² or kg

Default Value

0 kgcm² or kg

Data Type

Float
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
AXIS1.LOAD.INERTIA

5014h

01h

Unsigned32

-

1000:1

Read/Write

No

AXIS2.LOAD.INERTIA

5114h

01h

Unsigned32

-

1000:1

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.LOAD.INERTIA

5700

1644

Unsigned32

Read/Write

-

AXIS2.LOAD.INERTIA

71236

1164

Unsigned32

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.LOAD.INERTIA

5700

Float

Read/Write

-